Reports: Russian contractors killed by US strike in SyriaFebruary 13, 2018 6:33pm

MOSCOW (AP) — An unknown number of private Russian military contractors were killed by a U.S. strike in Syria, Russian media reported Tuesday in a development that could further inflame Russia-U.S. tensions.

Officials in both Moscow and Washington remained coy about the deaths, which would be an embarrassment for both countries if it turns out that Russian fighters were part of a unit that attacked a military force with American troops.

President Vladimir Putin's spokesman, Dmitry Peskov, refrained from commenting on reports about the incident last week, saying they need to be verified.

Asked during a conference call with reporters if Putin raised the episode during a phone conversation Monday with U.S. President Donald Trump, Peskov said the situation in Syria wasn't discussed during the call.

Defense Secretary Jim Mattis said Tuesday that Russia has told the U.S. there were no Russians in the area of the strike. Mattis said he saw the news reports about Russian contractors possibly being casualties of the bombing.

"I don't have any reporting that some non-Russian Federation soldiers, but Russian contractors were among the casualties," Mattis told reporters traveling with him in Europe. "I can't give you anything on that. We have not received that word at Central Command or the Pentagon."

Russian media said the Russian private contractors were part of pro-government forces that advanced on oil fields in the eastern Deir el-Zour province and were targeted by the United States. The reports cited activists who confirmed that at least four Russian citizens were killed in Syria on Wednesday.

During the war in Syria, Russia and the United States have maintained a communications channel to avoid collisions between their warplanes and soldiers in the chaotic battlefield. If Russian deaths from the U.S. strike are confirmed, it would mean the two countries were on the verge of a direct military confrontation in Syria.

The episode could further strain ties between the two countries, which have plummeted to the lowest levels since the Cold War over the Ukrainian conflict, the war in Syria and the alleged Russian meddling in the 2016 U.S. presidential election.

The U.S. military said last week it unleashed air and artillery barrage on Syrian government-backed troops after some 300 attackers launched what appeared to be a coordinated assault on Syrian opposition forces accompanied by U.S. advisers in the province of Deir el-Zour. It said it was in regular communication with Russian counterparts before, during and after the attack, and Russian officials assured coalition officials they would not strike coalition forces.

It said the U.S. strikes, which reportedly killed about 100 of the attackers, were in self-defense.

The Russian Defense Ministry has insisted that its troops weren't involved in the incident, saying 25 Syrian volunteers were wounded in the U.S. strike.

It also noted pro-government forces that advanced toward the area under control of the U.S.-supported forces had failed to coordinate their action with the Russian military in Syria.

Mattis last week dismissed any suggestion that Russia had any control over the attacking force, whose nationalities, motives and makeup he could not identify.

The U.S. strike came as U.S.-backed Kurdish-led forces were vying with Russian-backed Syrian troops that are reinforced by Iranian-supported militias for control of the oil-rich Deir el-Zour province.

The Russian Defense Ministry charged that the Feb. 7 incident reflected a U.S. push to grab Syria's economic assets under the cover of fighting the Islamic State group.

Without mentioning the U.S. strike, Russian Foreign Minister Sergey Lavrov noted Tuesday that "Americans have taken dangerous unilateral steps."

"Those steps look increasingly as part of efforts to create a quasi-state on a large part of Syrian territory — from the eastern bank of the Euphrates River all the way to the border with Iraq," he said.

The state Tass news agency on Tuesday cited Natalya Krylova, a municipal lawmaker in the town of Asbestos in the Urals, as saying local residents Igor Kosoturov and Stanislav Matveyev were killed in Syria Wednesday.

The Interfax news agency said that the Cossack group in the westernmost Kalningrad region said a member named Vladimir Loginov was killed in combat in the province of Deir el-Zour. It also quoted Alexander Averin, leader of extreme leftist group Another Russia, as saying that one of its activists, Kirill Ananyev, was killed by the U.S. strike near Khusham.

Russian media also cited unconfirmed claims that overall casualties could have been as high as 200 and Russians could have accounted for the bulk of them. Those claims couldn't be verified.

Liberal politician Grigory Yavlinsky, who is running for president in Russia's March 18 presidential election, urged Putin to come into the open regarding the deaths of Russians in Syria, saying that official silence on the subject was "unacceptable."

"If many Russian citizens were killed, officials, including the commander-in-chief, must tell the nation about it and determine who is responsible for that," he said.

Russia has waged a military campaign in Syria since September 2015, helping Syrian President Bashar Assad's government seize large chunks of territory and turn the tide of war into its favor.

Russian media have reported that in addition to Russian servicemen deployed to Syria, thousands of Russians also fought there as private contractors, most serving with the so-called Wagner group. The private fighters allowed the Kremlin to keep the official death toll from its campaign in Syria low and avoid the negative public perception of its involvement in Syria as Putin is running for re-election in the March 18 vote.

The Kremlin and the Russian Defense Ministry refused to comment on media reports on Russian private contractors in Syria.

While the U.S. has used private contractors in Iraq and Afghanistan for years, Russian law forbids the hiring of mercenaries or working as one even though Russia has used proxies in eastern Ukraine, where it has backed pro-Moscow separatists since 2014. Some Russian lawmakers have called for legislation that would set rules for private military contractors.

___

Lolita C. Baldor in Rome contributed to this report.

Page 1 of 1

More Stories Like This

FILE - In this file photo taken on Monday, March 14, 2016, anti-corruption activist Lyubov Sobol talks to the Associated Press in Moscow, Russia.TLyubov Sobol who led the investigation for the Foundation for Fighting Corruption told The Associated Press that the ease with which Prigozhin has dodged probes and accusations testifies to his special place at the Kremlin: "He is under Vladimir Putin's protection and is beyond reach for police and courts in Russia." (AP Photo/Alexander Zemlianichenko)
Russian indicted by US seen as doing favors for Putin
UN vote expected on 30-day cease-fire in Syria to help needySweden and Kuwait called for a vote Thursday on a UN resolution ordering a 30-day cease-fire throughout Syria to enable to delivery of humanitarian aid to millions of people in acute need, and the evacuation of the critically sick and wounded
In this photo released on Wednesday Feb. 21, 2018, provided by the Syrian Civil Defense group known as the White Helmets, shows a member of the Syrian Civil Defense group, searches for victims under the rubble of a destroyed house that attacked by Syrian government forces airstrike, in Ghouta, a suburb of Damascus, Syria. New airstrikes and shelling on the besieged, rebel-held suburbs of the Syrian capital killed at least 10 people on Wednesday, a rescue organization and a monitoring group said. (Syrian Civil Defense White Helmets via AP)
Hospitals overwhelmed by bombing blitz of Damascus suburbs
FILE - In this May 23, 2017, file photo, Sheldon Adelson arrives for President Donald Trump's speech at the Israel museum in Jerusalem. Adelson has proposed paying for at least part of the new U.S. embassy in Jerusalem, four U.S. officials told The Associated Press, and the Trump administration is considering the offer. Lawyers at the State Department are looking into the legality of the highly unconventional proposal to cover part or all of the embassy’s costs through private donations, the administration officials said. (AP Photo/Sebastian Scheiner, File)
AP sources: Adelson offers to help pay for Jerusalem embassy
The Latest: Russia's amended Syrian UN resolution circulatedThe Latest: The United States is accusing Syrian President Bashar Assad of planning "to bomb or starve" opponents in the besieged Damascus suburbs of eastern Ghouta into submission
Trump again attacks Obama over RussiaPresident Donald Trump is again attacking his predecessor, suggesting he should have done more to prevent Russian election meddling
AdChoices

Related Searches

Related Searches

AdChoices