Latest nor'easter could dump a foot or more of snowMarch 12, 2018 10:06pm

BOSTON (AP) — Winter-weary New Englanders are preparing for blizzard conditions, more than a foot of snow and high winds as the third major nor'easter in two weeks bears down on the Northeast.

The National Weather Service on Monday issued a blizzard warning for much of the Massachusetts coast, a winter storm warning for most of New England and a winter weather advisory for portions of New York, Pennsylvania and New Jersey.

The storm is expected to hit late Monday and last through most of the day Tuesday, with snow accumulating at a rate of 2 inches per hour during the Tuesday morning commute, disrupting road and air travel. American Airlines announced that it had suspended all flight operations from Boston Logan International Airport on Tuesday because of the storm. The airline said arrivals and departures from Bangor, Maine, Burlington, Vermont, Manchester, New Hampshire and New Haven, Connecticut also will be shut down.

Amtrak said it is suspending service from Boston to New York's Penn Station on Tuesday until 11 a.m.

While the first two storms of the month brought coastal flooding and hundreds of thousands of power outages, this winter monster is a little bit different.

"This one's main impact is going to be snow," said Kim Buttrick, a meteorologist with the National Weather Service office in Taunton, Massachusetts.

More power outages are possible, but they are not expected to be as widespread as last week. Only minor coastal flooding is possible.

The blizzard warning means sustained winds of greater than 35 mph (56 kph), along with visibility of less than a quarter mile for prolonged periods, according to the weather service. Wind gusts as high as 65 mph (104 kph) are forecast in coastal areas.

Boston and eastern Massachusetts, as well as Rhode Island, could get a foot and a half of snow, with less to the west of the city.

Officials said Boston and Providence schools will be closed on Tuesday.

Maine also is bracing for a hard hit. The Portland International Jetport has had 75.5 inches (1.9 meters) of snow, far above the normal for the date of 51.8 inches (1.3 meters) with another 12 to 18 inches is on the way, said James Brown, of the National Weather Service.

In New Hampshire, where as much as 14 inches of snow is forecast, the storm is wreaking havoc with the age-old town meeting tradition. But Secretary of State William Gardner and Attorney General Gordon MacDonald said under state law, town meeting elections must go on.

In New York, heavy, wet snow is forecast for Long Island, which could get 5 to 10 inches of accumulation, while 2 to 4 inches are possible in New York City.

In New Jersey, the storm is expected to start out as light rain before changing over to all snow by early Tuesday, leaving behind up to 4 inches.

The Northeast isn't the only area of the country dealing with winter weather. As much as 15 inches of snow has fallen in a narrow band stretching from central Kentucky through southern West Virginia.

Most of North Carolina also is gearing up for snow, with spring a little more than a week away. Forecasters say up to 6 inches of snow is possible around Boone in the northern mountains, while other areas of the state should get only about 2 inches.

"Hopefully this will be the final punch of the winter," Buttrick said.

Page 1 of 1

More Stories Like This

Construction workers excavate and widen Brays Bayou as part of a nearly $500 million flood control project Thursday, March 22, 2018, in Houston. The project, which will widen 21 miles of the bayou and build stormwater detention basins, has proceeded in fits and starts for more than 20 years due to inconsistent funding. The project is one of several large-scale flood control projects Houston-area officials are hoping to fully fund and build thanks to billions of federal dollars that have been allocated to pay for flood mitigation efforts in the wake of Hurricane Harvey.  (AP Photo/David J. Phillip)
7 months after Harvey, flood-control projects' fate unclear
ADDS TITLE SENIOR DEPUTY - Senior deputy Jeff Farmer with the Santa Barbara County Sheriff office checks the Montecito Creek to make sure it is flowing correctly Thursday March 22, 2018. A powerful storm spread more rain across California on Thursday, flooding streets and threatening to unleash mud and debris flows into communities near areas burned bare by wildfires. (AP Photo/Daniel Dreifuss)
Powerful storm brought much-needed rain to California
Winter Arctic sea ice again grew far less than normalThe National Snow and Ice Data Center on Friday reports that crucial Arctic sea ice had a weak winter for build-up
Expert: Coolers made it worse in nursing home where 12 diedAn expert witness testified that portable coolers actually made things worse in a Florida nursing home where 12 patients died without air conditioning during Hurricane Irma.
Champ on the pole after weather washes out qualifyingWeather washed out qualifying for NASCAR's first stop this season at a short track and Martin Truex Jr. will start Sunday from the pole at Martinsville Speedway
Early spring snow and floods bring havoc to BalkansHeavy snow and flooding wreak havoc across eastern Europe on Friday, closing down roads, flooding homes and stopping ferries at the Adriatic coast

Related Searches

Related Searches