Alabama trooper says the driver is the person killed in the bus crashMarch 13, 2018 3:09pm

LOXLEY, Ala. (AP) — Alabama trooper says the driver is the person killed in the bus crash.

Page 1 of 1

More Stories Like This

ADDS TITLE SENIOR DEPUTY - Senior deputy Jeff Farmer with the Santa Barbara County Sheriff office checks the Montecito Creek to make sure it is flowing correctly Thursday March 22, 2018. A powerful storm spread more rain across California on Thursday, flooding streets and threatening to unleash mud and debris flows into communities near areas burned bare by wildfires. (AP Photo/Daniel Dreifuss)
Powerful storm brought much-needed rain to California
The Latest: FBI says air base crash has no known terror linkInvestigators say a van that illegally entered a Northern California Air Force base this week was on fire as it approached the gate.
Sean Ragan, FBI special agent in charge, briefs reporters about a crash at the main gate of Travis Air Force Base, Calif., Friday, March 23, 2018. A 51-year-old man drove a flaming minivan loaded with propane tanks and gasoline cans through the main gate of the major Northern California Air Force base, authorities said, but added the driver had no known links to terrorism. (AP Photo/Jonathan J. Cooper)
FBI seeks motive for fiery van crash at California air base
Driver dead after crashing at California Air Force baseOfficials say a driver breached the main gate at Travis Air Force Base in Northern California, then crashed and died
Nissan Chief Planning Officer Philippe Klein speaks to journalists during a media roundtable at Nissan headquarters Friday March 23, 2018 in Yokohama, near Tokyo. Nissan's chief planning officer said Friday the Japanese automaker does not plan to change its road tests for self-driving vehicles after the recent fatal accident of an Uber autonomous vehicle. (AP Photo/Yuri Kageyama)
Nissan not changing autonomous drive tests over Uber crash
In this Thursday, March 22, 2018 photo, Woody stands on the dock that he jumped from the day before in which he rescued Mason Ringer from the Okatie River, in Okatie, S.C. The dog jumped into the choppy, 58-degree (14 C) water on Wednesday and pulled Ringer, who was struggling after his boat had capsized, toward a nearby dock.  (Drew Martin/The Island Packet via AP)
True retriever: Dog plucks flailing man from river

Related Searches

Related Searches